Our new layout with the TPA2013 boost/amplifier IC has a problem.
The boost section works fine (3Vin and 5.5Vout) but the amplifier outputs remain at ground even with 1Vpp input signal. The two active low shutdown pins are both driven high and boost is working so presumably the amplifier should be on. The input signal is single ended sine 1Vpp 500Hz into the IN+, the IN- is grounded, both through 1uF caps. The load is 4 ohms through LC filters as shown in the datasheet.
Has anyone else had trouble like this? Any advise would be appreciated.
Thanks JT