Other Parts Discussed in Thread: SRC4190
Hi,
I am searching a SRC to convert I2S audio sample rate in our design.
SRC4190 seems meet our requirement:
There is a HDMI Rx in our board and it capture HDMI audio as I2S signal(sample rate range: 32KHz ~ 192KHz). The I2S audio need to be converted to 48KHz or 44.1KHz before enter to our audio codec(for mixing multi analog and digital audio signal). Block diagram as below:
HDMI Rx -> SRC->Audio codec
audio input : I2S sample rate from 32KHz to 196KHz
audo output: 44.1KHz/48KHz
Please help me check:
(1) SRC is set both input and output slave mode, so the BCKI and LRCKI is provided from HDMI Rx and BCKO and LRCKO is from audio codec. RCKI is must for SRC4190 as reference clock(from Crystal Oscillator), is it right?
(2) Auto resample is done when input/output clock is actived? There is no additional configuration for resampling?
(3) The sample rate range of HDMI audio source is 32KHz~196KHz. So all sample rate in the range could be resample to 44.1KHz or 48KHz?
(such as 32KHz->44.1KHz, 48KHz->44.1KHz, 96KHz->44.1KHz etc...I know that max sample rate range is 4KHz~212KHz in SRC4190 and ratio is 1:16)
(4) The sample rate ratio 1:16 means when input sample rate is 4KHz, it could be resample to maxmium 4x16=64KHz, so 4~64KHz output sample rate is available?
Thanks!
BR,
Steven