Hello,
Hopefully someone can point me the right way. I'm using a TLV320AIC3254EVM-U development "stick" to create a processing block for an intercom system. Got algorithms that should do the job, used the script utility so that it boots the app on startup, all that works even when plugged into a Linux machine with no drivers running. Problem is, to test the application in the field I need to get the '3254EVM-U modules to run all by themselves using just 5V power, with a minimum of extra stuff to make them go.
So the question is - Is there any way to trick the '3254EVM-U into thinking it's plugged into a PC so it'll boot up and run the script loaded into it? Sure would make my day. Thanks for any pointers.