I'm conducting EMC testing fro my design using Class D audio amplifier. (Actual device is TAS5615DKD). The board has been carefully laid out to minimise RF emissions. However emissions are high enough to fail the CE and FCC requirements particularly in the range of 55-200 MHz region. I'm carrying out a few modifications to the circuit to try to reduce emissions. In the mean time has anyone been involved in reducing emissions from a class D amp and can let me know what modifications they have made so I can also try these as well? Thanks.