Other Parts Discussed in Thread: PCM2912A
Hi Ivan,
Creating a separate thread for this discussion.
Previous thread:
I got the DEM-PCM2912A board. I am trying to use the board with microphone from sound professionals
Microphone link: http://www.soundprofessionals.com/cgi-bin/gold/item/SP-MMM-1
I tried on linux but there was no output from aplay. So I connected in windows and followed the instructions inPCM2912a user manual by changing the settings in control panel. The red light for microphone input will be ON but I am not able to record any audio from the board Mic in. The microphone is working fine when connected to laptop Mic in. So I was wondering if there are any restrictions w.r.to DEM-PCM2912A microphone input.
Please let me know.
Further today I checked the voltage at TP14. I get around ~1.65V. So I was thinking microphone is not getting enough power to capture data. Please confirm if the voltage input for microphone that I am observing is expected one.
Thanks
Sandeep