I'm having trouble getting the TPA2100P1 amplifier to work correctly. I'm getting a 14 Vpp 265 kHz square wave output with a 100 mVpp 1 kHz sine wave input. A .82 uF cap is connected between the outputs to represent the speaker. I noticed that the supply current was 40 mA at 3.6 V which is higher than specified in the datasheet. Any troubleshooting ideas?
Thanks