(replied to a old post but not sure if anyone will see it, so posting a new thread)
I am unable to get PurePath Studio (Home Audio) to download or configure my EVM.
As noted in the previous threads about this issue, the EVM I received does not have any pull down resistors on W3. Jumpers are removed from W3 - 6,7,14 and I installed pull down resistors on TP6,TP7 and TP14, however I am still receiving the following errors while attempting to load or connect:
--------------
Build succeeded.
Found board type: FWIDPCM5101EVM-S.
Board sampling rate: 48000Hz.
Downloading base_main_Rate48.cfg to the EVM.
Application download failed. Error: Unable to connect to hardware
-------------
Please advise, I am on a tight deadline and need to get this EVM working.