This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I made a simple PCM2704 dac, it worked but there is a serious problem, i can hear a buzz sound that that's very annoying. Then i plug it in my QA400 and here is the result:
[IMG]i.imgur.com/.../IMG]
The DAC connect to QA400 with 10kohm load, no signal playing, that buzz is clearly visible at around 9khz and 18khz
[IMG]i.imgur.com/.../IMG]
Dac playing -2.5dbfs
This is my layout, hope some one can help me to find out the problem.
Hi Thai,
I added some notes to one of your design images.
I'm concerned about the GND polygons. One has DGND and ZGND connected directly and the other has AGNDL, AGNDR and PGND. ZGND is ground for internal regulator and all the supply rails decoupling capacitors are connected to the other set of GND; besides PGND is ground for DAC, OSC and PLL and this is not connected directly to the crystal oscilator circuitry. It seems that both ground polygons are connected on a single point by a resistor or ferrite bead but maybe this connection is not strong enough to let the device work fine. Some times a bad ground connection causes noise issues.
You could use the PCM2704C EVM design as reference.
Best regards,
-Ivan Salazar
Texas Instruments