This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where can I find the full description of TAS5754M register map?

Other Parts Discussed in Thread: TAS5754M

Hi,

I'm looking for fully register map of TAS5754M full register map.

I've read the data sheet. A lot of page of register map is not described in data sheet.

I'm trying to implement a simple EQ application. The TAS5754M is controlled by external MCU through I2C.

For example, MCU will send I2C command to write 5754 register for add 1db gain of 1KHz frequency.

It said that "Integrate dynamic controls (such as volume controls, mute commands, and mode-based EQ curves) into the main system program." in data sheet.

So, is there any way to implement frequency-based EQ controls.

  • Hi,

    Welcome to E2E, Thanks for your interest in our products!.

    The Register maps corresponding to the audio processing blocks of the TAS5754/56 are not really located into a specific location as the features of the amplifier changes between different HybridFlows. So each hybrid flow has a different arrangement of available locations used to implement the different processing blocks. I would suggest you to use PurePath console and load the desired Hybrid Flow, then modify a feature like an equalizer and see which register is modified by the use of the logging tool.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Hi Diego,

    Thanks for your reply.

    I will adopt your suggestion.

    Thanks

    Damon