Hello,
I had a question about the current requirements for the analog and digital supplies of the TAS2505. I see the following excerpt in the datasheet:
The TAS2505 has a built-in LDO which can generate the analog supply (AVDD) also the digital supply
(DVDD) from input voltage range of 2.7 V to 5.5 V with high PSRR. If combined power supply current is
50 mA or less, then this LDO can deliver power to both analog and digital power supplies. If the only
speaker power supply is present and LDO Select pin is enabled, the LDO can power up without requiring
other supplies. This LDO requires a minimum dropout voltage of 300 mV and can support load currents up
to 50 mA. For stability reasons the LDO requires a minimum decoupling capacitor of 1 μF (±50%) on the
analog supply (AVDD) pin and the digital supply (DVDD) pin. If use this LDO output voltage for the digital
supply (DVDD) pin, the analog supply (AVDD) pin connected to the digital supply (DVDD) externally is
required.
I don't see any data on the current requirements for the analog or digital section. Is the current requirement driven by how the device is configured? Would it be a better solution to use external supplies?
Thanks so much for your help!