Other Parts Discussed in Thread: TAS5760M, TIDA-00404, TAS5754M
Dear,
We are looking for a 2.1 loudspeaker solution with suitable audio Amp system. I think TI can support the requirement with tis resources. Some information are attached as below:
L/R loudspeaker is 4 Ohms and 15W as rated power.
Bass is 4Ohms and 30W as rated power.
Supply is 12V DC.
Checked in TI design, I find it seems ok but the supported power may be a little lower.
具有信号处理功能的 2.1 D 类数字输入闭环音频放大器系统参考设计
(正在供货) TIDA-00404
Could you help recommand an adaptive solution for 2.1 loudspeaker listed above?
Br & Thanks!