Hi,
Some time ago I saw a post of a user struggling with using CP2114 with PCM1794A. He mentioned he used PCM2707 to drive it with the success, however it doesn't seem to be a matching component as:
- it is also a DAC (so why using DAC to drive other DAC?)
- it only supports clocks up to 48kHz which is the main no-go for me.
So, does TI recommend any other chip working with clocks up to 192kHz and compatible with PCM1794A?
Thanks, Radek