Other Parts Discussed in Thread: TAS5760M, TAS5710, TAS5754M
Hi,
Let me ask you some questions about Class-D closed loop by comparing between TAS5710,TAS5754M and TAS5760M as below.
1) I thnik that TAS5710 and TAS5760M are "pure class-D amp" but TAS5754M is not pure.
Because TAS5754M consists of "DAC+Class-D" and PWM signal is made from analog audio signal (from DAC).
In other words, TAS5754M is analog input class-D amp.
Is my understanding correct?
2) I think the performance of both TAS5710 and TAS5760M looks similar.
So I suppose the both arechitecture of "Closed Loop Class D Amp" seems to be same or very similar.
Is this correct?
3) About "closed loop", the feedback PWM signals are from "H-Bridge FET" out, right?
And is the feedback PWM signal compared to input PWM signal? (Analog comparison)
Or the feedback PWM signal is "LP filtered + A/D converted" and compared to input digital audio signals??
4) TAS5754M performance
Though TAS5754M is using Analog signal to make PWM signal, the TAS5754M performance seems to be better than TAS5710/5760M.
I do not understand well the reason why...
The signal path of "Digital Audio data ---> DAC ---> Analog Audio data ---> Analog PWM" seems not to be better than all digital signal processing.
The reason of the good performance is DAC performance of TAS5754M, right?
Thank you for your support!
Best Regards,