Other Parts Discussed in Thread: TLV320ADC3101
Hi,
We are facing an issue that the audio we sample has a slight (positive) offset . (I am talking 0.015 on a scale of -1..1 in linear scale)
We only connect the signal through a capacitor (AC coupled) to the chip, and we can see that the chip drives the voltage at 1.35V. Grounding the pin clearly clips the measured signal all the way negative, so it seems to be driven sighly higher than the ADC expects.
(Attaching a scope (1Mohm input resistance) already changes the measured offset so significantly, that it is hard to see the exact signal directly on the pin.)
=> Is it possible to calibrate the ADC somehow, to compensate for the offset?
Thank you for your reply!
Arnout