So i am hoping this is a simple couple of questions:
can we connect the ADC/DAC to a DAA phone line interface circuit without any components in between? the DAA circuit we are using is CPC5622A. it looks like it has a high impedance for inputs/outputs (600Ohm) and i was wondering if the codec can handle that on any of it's particular inputs/outputs.
in addition we will be using a 150Ohm speaker for a handset and we want it to be able to get LOUD. is the HP Out path too much and we should use a line out or is HP out a better match for this kind of speaker?
thanks