Other Parts Discussed in Thread: LM4673
This design uses an LM4673 with 47uH series inductors on each output pin and 0.1uF to ground on the load side of each inductor for EMI filtering. PVDD, AVDD and SHDN are wired together to 3.3V and bypassed to ground with 10uF X7R. Both inputs are AC coupled and the source impedance driving each is about 7.5K. The output circuit has three possible load configurations: Open, 500 ohm and 4 ohm speaker.
This circuit is implemented now in two prototypes and so far we have experienced four failures. The failures are all the same. Both output lines stop switching and appear to float at around 300mV. The supply current to the part is constant at about 30mA.
I have verified that there is no overshoot on the 3.3V supply during power-up. The circuit is operating with enough gain to result in clipping with some signals.
I have not yet established any pattern for when the failures occur. In some cases the parts failed almost immediately on power-up and in others they operated as expected for weeks.
Does anyone have any insight around why this is occurring? My best guess is that the output filters are causing the output clamp diodes to carry more current during commutation than with a direct speaker connection, especially when there is no load. Waiting on more parts to test this theory by installing external schottky clamps.