We are working with the PCM1864EVM and we need to pass a 30kHz signal through it. The signal we get out is heavily filtered, so we think that the board is set at the lowest sampling rate of 48kHz. We were trying to use the PurePath GUI to change the sampling rate to 192kHz through the "Block Diagram" page, but we do not think that the settings were being saved because the output was still degraded. If we change the sampling rate to 192kHz, when we open up the window again it always has switched back to 48kHz.
We want to send the 30kHz signal through with minimal filtering. What is the best way to change the sampling rate of the board? And are there any filters that can be changed or turned off so that the board will not destroy our 30kHz signal?