How do I interpret the t(DOD) parameter for the PCM audio interface (i2s) when operated in slave mode? (see pg 19, Figure 24 of PCM3060 data sheet for example). The text description for this parameter is "DOUT delay time from BCK1/2 falling edge".
Does this parameter mean data is valid on the DOUT pin between the min and max (15ns and 70ns for the PCM3060)? Or does it mean that data can take this long to setup on the DOUT pin (and is only safe to read outside this window)?
Thanks