Other Parts Discussed in Thread: TPA3251, TAS5631B, TAS5630B
Dear,
I want to build high end class d audio amp.
Request:
Output: 8ohm - 500-600W per channel
Extra Low THD
Analog input (Digital input, but this is not important)
Output channel: 2-4
Can I realize this amp with TI chips or I must add AB MOSFET?
Solution with MOSFET is acceptably...
This is nice solution with MOSFET and BIAS controller but it is outdate:
With respect
Marko Jankovic