Other Parts Discussed in Thread: TAS3103, TAS3204, TAS5613
ll
Hello
I am an embedded systems and power electronics engineer.
I am also and avid AV enthusiast and hobbyist
But hands on experience in audio is limited to only about five projects
I wanted to get my hands dirty with class D amps from TI.
I recently ordered a variety of Purepath Dsps and class d amplifiers for playing around
I first wanted to build a TAS5613 based amplifier and then go on to playing around with TAS3204 and TAS3103
I am in the process of designing the TAS5613 amp however there were some parts unclear to me in the datasheet
For the oscillator section which says OSC_IO+ and -
1. am i right in assuming that the pins need to be connected to a regular crystal with load caps?
2. If yes , then what is the crystal frequency?
3. If no , then how do i provide a clock input to the TAS5613