I've been burning up a few of these chips somehow, and am uncertain why. They are used exactly as in the datasheet (mono mode), and I'm not driving them terribly hard. But during testing, from time to time, the amp just fails, shorting both outputs to ground. PVDD is 24V, running at 192kHz.
Our load is a little unusual but well within the published specs.
Since there is DC, overvoltage, and thermal protection, what condition could get around them, and cause a failure? Maybe a spurious discontinuity in the input signal? Any other oddball load characteristic it's sensitive to?
It works sometimes, but not reliably, so hints in tracking this down would be helpful.