Hello,
I am looking to use the LM567 tone decoder circuit. I believe I have followed all of the steps on the datasheet correctly. I set the center frequency using 1.1/(R1*C1), and then I set the bandwidth using table 2 and the center frequency in kHz. However, after I follow this procedure the output of the circuit does not change.
Note that I use C2=1uF, C3=2.2uF (both ceramic), Cin=1uF, Ro=27kOhm, C1=0.1uF and R1=314ohm and Vcc=5V. Also I am using a somewhat idealized input waveform at the moment, in an attempt to just get the output to behave correctly. It is a 35kHz sinusoidal waveform with a peak voltage of 2.5V. I try both pulsed wave and continuous wave, but neither seems to work. Any help would be much appreciated.
Mike