Dear Technical Support Team,
I have a question about audio DAC.
Can I use audio DAC instead of precision DAC for precision application?
I'm searching for 24bit and 2ch or 4ch DAC on precision DAC.
I can't find it. but audio DAC has these spec like PCM1780/1781 and PCM1753/1754.
I think that audio the DAC doesn't have offset spec.
Do you have the other difference between audio DAC and precision DAC?
Could you give me some attention when we use it?
・Resolution:24bit
・Channels:2~4ch
・Sample Rate(MAX)(SPS):144kSPS
・I/F:PCM Data format
Regards,
ttd