This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AUDIO DAC

Guru 13485 points

Other Parts Discussed in Thread: PCM2706, DIR9001, PCM5102A

looking for stereo audio D2A with SPDIF input and analog outputs. Volume control in the output is nice to have feature

  • Hi, eli,

    Please take a look at the possible devices below:

    PCM2906: This is an audio codec that supports SPDIF input and output. Basically, the SPDIF is converted to USB and vice versa. It also supports analog input and output.
    PCM2706: This is an audio DAC that supports all your requirements except the SPDIF input. This device only supports SPDIF output.

    Please take a look at these devices and let me know if you have questions or comments.

    Best regards,
    Luis Fernando Rodríguez S.
  • Hi Eli,

    you can use combination of S/PDIF receiver DIR9001 and some DAC like PCM5102A. VOLUME control is not possible on the digital side. You can control volume with potentiometer on the analog side.

    best regards,

    Pavel.