This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3101 Headphone out put can we can we bypass to class-ab amplifier to use external class D-amplifier for connecting 10W Speaker

Other Parts Discussed in Thread: TLV320DAC3101

Hi,

We are using TLV320DAC3101 Audio DAC ic . Our requirement should be cater for below requirements.

1. Headset(Class-AB)

2. Class-d amplifier output for 8E/0.5W speaker

3. External 10W speaker.

In TLV320DAC3101 IC we have option for Headphone output or Line out put on same pin out. I understand that selection can be from software. When i select line output is this class-AB amplifier will be bypassed?It is not shown more clearly in datasheet architecture is this correct?

  • Hi, Sudheer,

    Welcome to E2E and thank you for your interest in our products!

    The TLV320DAC3101 outputs can be enabled or disabled independently. Basically, if you don't need to use a specific output, there's no need to connect the DAC output to that output. Additionally, the driver can be disabled even if the DAC output is routed. If you require a lineout-drive mode, you would need to write 11 to page 1 / register 44.

    Best regards,
    Luis Fernando Rodríguez S.