Other Parts Discussed in Thread: PCM9211, DSD1792A
I would like to use the PCM9211 in hardware control mode. If I purchase the evaluation board as a starting point. How do I.
1 Select which optical input is being used
2 Connect a USB module such as the MIKROE-1204 click board (Found on Mouser)
My end desire is to connect the PCM9211 to the DSD1792A and have the ability to have a COAX, USB and 1 more more optical inputs. I would like to run everything in default (Hardware) mode with no processor control.
Thank you