This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48511 output is abnormal

Output RMS value is just 500mV. Target value is more than 4.4V.

Below is our schematic.

VBATT:4.2V, VDD_LM:7.8V

Input signal is single input.(CDC_HPH_REF is analog ground)

With the same input signal using AW8733(AMP) output RMS value is 4V.

Please tell me how can i debug LM48511 in this case.