Hi,
Could you please give me the DAP latency except ASCR latency ?
Is my understanding correct that I believe that it is 20/FSout ~ 25/FSout ?
Best regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sadanori-San,
It is very hard to specify this latency because it depends highly on the filters, settings, and processing selected. It also depends on the sampling rate of the input. Where did you read the 20-25/FS value?
Why does the customer need this info?
Regards,
-Adam
Hi Adam-san,
Thank you for your reply.
It is necessary to understand the propagation delay and adjust the phase using the rip-sync delay IC such as TPA5050 if using each different part as the pwm modulator for main audio board and sub-board(e.g. subwoofer)
I have heard this information as TAS5538 from your local FAE, unfortunately he no longer works at TI.
So, I understand that TAS5548 is same with TAS5538 except the ASRC function and the latency also depends on the audio processing configuration.
Best regards,
Kato
Hi Adam-san,
Could you please give me the latency for the following condition ?
<Condition for TAS5548>
- High pass : Enabled
- Biquad coefficients : Set to all pass
- Bass and treble bypass/inline : Bypass
- DRC bypass/inline : Bypass
- Loudness : Disabled(default values)
- AM interface mode : Disabled
Best regards,
Kato
Hi Adam-san,
Please let me know if you have any updates on my request.
Best regards,
Kato