(I am partly translating from Japanese to English using google translation. Thank you google awesome google)
I think that English can be understood from those who do PPAP.
I have less experiences this PCM5242RHBEVM contained PCM5242.
Please help me please.
I want to make an APC router that the staff uses around the studio inside the FM radio broadcasting station.
When broadcast signals are switched from two kinds of systems, I want to connect with fade-out fade-in with I 2 S signal as it is
Therefore, I want to use an IC with the following functions. If this IC has its function
Does PCM5242RHBEVM contained PCM5242 have the function of Change Volume I2S to I2S Signal ?
then
Could you teach us procedure or procedure URL what
How to control this IC with a microcomputer and PurePath™ ?
The final product is controlled with a microcomputer such as Nios II built in the MAX10.
Please I hope Post on the net what Universal sample code ,sample Universal Electronic circuit and so .
thank you for reading Arigatou.