Dear Sirs,
My customer asked us about timing requirement specification.
When they confirmed with actual board equipped with PCM 1795, they were out of specifications with the following items.
1.Data hold time(t(D-HD) Spec(Max):900ns ⇒ 996ns2.Fall time of SCL / SDA signal(t(SCL-F) (t(SDA-F) Spec(min):20 + 0.1 CB ns ⇒ 8 nsSo please tell me the following questions. 1) When Data hold time becomes larger than prescribed max value What kind of problem is concrete?2) When the SCL / SDA Fall time becomes smaller than the prescribed min value What kind of defects can be considered concretely?3) Please tell me why Fast mode and Standard mode are set to the same.Best Regards,Y,Hasebe