Part Number: PCM1803
E2E,
We have an issue where a pop is generated when the battery is quickly removed from my audio product that uses a PCM1803, and we noticed that it improves if we place more capacitance on VREF.
The datasheet recommends a 10uF and a 0.1uF, but we are seeing a 100u in place of the 10u seems to help, but I wanted to know if there is any maximum capacitance values or any reasons we could or should not put this amount of capacitance on those lines. Also, should the caps on Vref1 and Vref2 be balanced? Can you clarify how do those supplies interact?
Best regards,
Matt