Part Number: PCM5242
I am using a multiple feedback lowpass filter to buffer the output of the PCM5242 as an interface to my discrete single ended input amplifier. I am finding that the buffer is actually adding noise to the output (reducing SNR), and modifying the buffer to single ended will reduce the noise by about 5 dB however now I have to add 6dB gain in order to get the signal where I need (thus adding 6dB of noise). The filter I am using can be found on page 36 of the following datasheet: http://www.ti.com/lit/ds/symlink/pcm1690.pdf , I have modified the values slightly for 0dB gain using filter pro desktop, ensuring that the input resistors are above 5K so I don't load the output of the DAC.