This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: TLV320ADC3101 Application Issue

Part Number: TLV320ADC3101

Dear Sir,

My customers Garmin uses DAC3101 found some issue need your strong help.

They using 2 differential pair - IN1L&IN1R  and IN2L&IN3L.

In this test, the frequency and strength of IN1L&IN1R is 1KHz and -11dB, and the frequency and strength of IN2L&IN3L is 1.5KHz and -17dB.

The test results are as below,

The channel with weaker signal strength (1.5KHz) is obviously affected by the stronger one (1KHz), which is unacceptable. 

We did the test in EVM, could you pls check why ADC3101 with this issue? Can we solve it?

Thanks, Ian.