This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760M: Control software for Latest PurePath Console Motherboard

Part Number: TAS5760M


Dear Team,

I get a new ppc mother board for customer but don't know which version PPC supports this, and when I push the mode/input/volume buttons on the board, no LED will light on.

The board is:

http://www.ti.com/tool/purepath-cmbevm

and I will use it with TAS5760M.

Please help,

Thanks a lot,

Kevin Dang

  • Hi, Kevin,

    PurePath Console Ver1 software (PPC1) is the GUI used to evaluate TAS5760M. The EVM requires PurePath Console Motherboard (PPCMB) as the interface between the GUI and Amplifier. Any version of PPCMB is compatible with the software and EVM.

    The controls you mention (volume, source, etc) are included in the controller board as an optional interface for standalone operation using the microcontroller used in the PPCMB (Please refer to TIDA-00609). This interface has no effect when the EVM is evaluated with PPC1.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer