Part Number: LM4860
The LM4860 amplifier is experiencing stability problems. In looking at the circuit and debug we had two specific questions we were hoping you could help on.
1) Pins 11 (Gain-out) and 10 (Vo1) appear to be the same point functionally from the block diagram. When measuring on an actual part, there is 35 ohms between 10 and 11. Is there an internal 35 ohm series output resistor on pin 10 for Vo1 (and pin 15 for Vo2)?
2) For a unity gain application, how much load capacitance can the amplifier drive without stability issues?
Thanks,
Jason