Other Parts Discussed in Thread: TLV320AIC3204
Hello,
I have a working TLV320AIC3204 PCB and I have been controlling the DSP settings with the MCU.
but I want to setup the whole configuration using EVM GUI first and write the final config into a code at the end.
When I tried to connect the I2C line between the 2 boards, I think it damaged my MCU, my original board is not working properly anymore.
My EVM USB interface is set to "I2C fast" and the board's IOVDD is also 3.3V.
I'm not sure what I connected wrong in the PCB.
Since they are both using 3.3V, I didn't connect the VDD and GND of PCB1 and EVM board.
Is it not possible to use the EVM to control external IC?