Hello Audio Folks, a customer is using TAS5731M. They get a problem on dis-continuous sound output in max volume output. If they set back reg 0x10 = 0x07, then it is OK with no problem.
They are using 12V supply. In data sheet, the requirement on setting reg 0x10 is only on 18V or higher supply voltage. That is the reason they don't set reg 0x10. However, one thing is that they are using very low impedance (two 5.6 ohm speaker in parallel, i.e. 2.8 ohm). So, the question is that the requirement on setting reg 0x10 is on high current or it is just required on high supply voltage.
Regards,
Kes