Dear, Sir.
My customer is considering to apply TAS2553 on their system.
PDM is not used on the system at this time.
So IVCLKIN pin will be non-used.
Please give your advice about the best connection for IVCLKIN non-use pin.
Best Regards,
H. Sakai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear, Sir.
My customer is considering to apply TAS2553 on their system.
PDM is not used on the system at this time.
So IVCLKIN pin will be non-used.
Please give your advice about the best connection for IVCLKIN non-use pin.
Best Regards,
H. Sakai
Dear, Ivan-san.
Thank you so much for your teaching & advice.
The customer is making additional question. Please give your advice again.
For VBAT bias, 4.5V/1A DCDC Converter is located.
1. 47page on the TAS2553 datashhet, VBAT max current is defined.
Is it a kind of peak current?
2. If the current was insufficient, What kind of issue was concerned?
For instance, the output sound pressure would be decreased. ]
Best Regards,
H. Sakai
Dear, Ivan-san.
I would like to double-confirm your mentioning. Sorry again & again.
I wonder "Protected" means that TAS2553 will be shutdown by VBAT battery monitor function block
such as battery tracking AGC or VBOOST output voltage will be decreased at insufficient current from the supply?
Best Regards,
H. Sakai
Dear, Ivan-san.
Thank you so much for all of your teachings.
It is first time for us to use TAS2553, Please teach more although it is quite fundermental.
1. PLL : DS page 16 & 17 described PLL CLK setting.
a) I think it to set the CLK source(MCLK, BCLK, etc) and generate internal DAC & ADC clock
utilizing divider. I wonnder my understanding is correct?
b) I think I-V sense is needed for Boost amp function. ADC should be utilized.
I wonnder my understanding is correct?
c) How much value will be reasonable as the sampling rate(? sps)?
Smart amp function will not be used. Expected as IS2 input & Boost amp.
2. Resister 0x02 bit1.
Smart amp function will not be used. Which setting enable/disable is correct as IVSENSE_EN?
3. Resister 0x03 bit3 ~ bit6.
Could you please teach the correct seeting for these four bits.
4. Resister 0x07 bit0 ~ bit7.
Could you please teach the correct seeting for these eight bits.
Best Regards,
H. Sakai