This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Absolute Max. Output current of LME49720

Part Number: LME49720


Dear Sirs,

My customer asked us about Absolute Max. Output current of LME49720.

So I checked the datasheet, but Absolute Maximum Rating of output current was not found.

Then Supply Voltage Range is stated in Absolute Maximum Rating on the datasheet page 3, and the value is ± 2.5 V ≤ VS ≤ ± 17 V.

In addition, the specifications of the Output Current to 5 pages of data sheets have been described, the condition has become to RL = 600Ω, VS = ± 17V.

From these two values, AbsoluteMaximumRating of the output current is

Output Current (Absolute Max.)=± 17 V / 600 Ω = ± 28.33 mA.

Is this value correct?

Best Regards,

Y.Hasebe