According to Section 3 of the Application Reference guides, and a post in this forum, IOVDD cannot rise before SPKVDD otherwise the LDO will not turn on. Is that true? I have two board supplies: SPKVDD at 5.0V and IOVDD at 3.3V. Now if the internal LDO supplies AVDD and DVDD from the SPKVDD, it seems very difficult for me to provide IOVDD between SPKVDD and the LDO outputs as required by the application reference guides. Is there some flexibility on when I apply IOVDD? Can it come after AVDD and DVDD? If not what is the recommended system design to ensure the right timing for IOVDD?