This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3262: Questions about EVM Application.

Part Number: TLV320AIC3262

Dear Sir,

Please kindly to answer below questions with using aic3262 EVM?

  1. I use Multi_Channel_Digi as AIC3262 output. I try to start recording audio file (.wav) but the audio format is stereo( only two channels).

What I want is a four channel audio file. Could you please advise how to implement?

 

2. I want to adjust two coeficient MDAC and MADC. Should I just modify the variable in systemsetting code editor?

 

Thanks, Ian.

  • Hi, Ian,

    1. Unfortunately, the TLV320AIC3262EVM-U cannot be used in multi-channel operations with the PC. PurePath Studio will configure the EVM in multi-channel mode, but the TAS1020b in the EVM only can be used for mono/stereo purposes. Even if the codec is configured correctly, the PC only can use the EVM in mono/stereo modes.

    2. Exactly, in order to modify the MDAC and MADC values, you only need to modify the system settings code in PurePath Studio.

    Best regards,
    Luis Fernando Rodríguez S.