This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48560: drive high load capacitance, high frequency

Guru 20090 points

Part Number: LM48560

Hello,

Can we use LM48560 on the following conditions? 

16kHz band width
5uF load capacitance
Vout 30Vpp (want )
The gain at 16 kHz is -20 dB or more with reference to the gain of 1 kHz. (want)

I have the evaluation data of my customer. In their evaluation, they couldn't get the gain above 10kHz.
Since the data is customer confidential, I can't post the data to this post.
Could you please contact to the following my address?

asaka-r@clv.macnica.co.jp

Best Regards,
Ryuji Asaka