This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS1020B max sampling rate

Hi all,

does TAS1020B support sampling rates bigger than 24bits/48kHz?  It looks like there is some problem with the Windows, that it can't support it very well - any ideas whether current win drivers fro TAS1020B can really support 48kHz/24bits?

 

best regards

Oskar

  • Hello Oskar:

    TAS1020 can go up to 96 kHz and is limited at 96 kHz due to memory limitation.

     

    TAS1020 has about 1.1kByte of RAM.

     

    2 channels * 3 bytes (24 bits) * 96 samples per mS * 2 (double buffering for synchronous isochronous transfer) = 1152 Bytes

     

    One of our colleagues did a timing analysis of the USB bus and saw that it only actually needs 935 bytes at anytime in the buffer.

    I have a document but cannot attach.  I will ask someone to help me loading this timing analysis here.

    Best regards,

    Tuan