I’m using this on a single 30V supply and am seeing considerable DC offset at the output when referencing the input to mid rail (15V). On the EVM, I biased the xIN+ pins to 15V with 20k resistors initially, but found reducing these to 5k helped considerably. Any comments on DC offset with regards to single supply operation would be appreciated.
Additionally, on the product we're developing, we are using the VQFN package. I cannot get it to output anything below the mid rail reference of 15V. Aside from the package change, the circuit appears identical to our EVM.