Other Parts Discussed in Thread: PCM1862,
Hello,
I wonder about the difference in minimal (80dBA) and average (92dBA) on this part. That difference is much worse than, say, PCM1862 has. At the same time, the FFT from the datasheets show only about 10dB difference between these two ADCs. on average values, that's about right. On minimal values, it is not.
The TLV320ADC3101 has features that PCM1862 does not have, and I would love to use it, but 80dB would not be acceptable in my application.
My question is - what is the nature of that 80dB SNR? is it low-frequency flicker noise (that I could possibly filter out), or does the SNR depend on the date code or the factory?
Also, is there data on SNR within 100Hz - 10kHz range?
Thanks!