This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3263: Program TLV320AIC3263 without evaluation board using CC3200

Part Number: TLV320AIC3263
Other Parts Discussed in Thread: CC3200,

Dear Community,

We are making a IOT based product using CC3200 

We have decided to include Voice integration to our product and give customers a seamless experience

How ever this is our first dive into the ocean of digital signal processing

The requirements of the voice processing are as follows

a. The blackbox must take voice input from 4 mics and perform some sort of active noise cancellation
b. The blackbox must have codecs ADC/DAC and support I2S protocol so its easily interface able with CC3200
c. The blackbox must be able to drive a small speaker 

Hence We have selected the TLV320AIC3263 with mini DSP ( Kindly correct us if this is wrong )

Here are my following concerns

1. How to program this DSP ? There is a Pure Path Studio to which we have obtained access, But We are currently unable to purchase the EVM board because of its high costs

2. Can we make the connections in Pure Path Studio and export the generated code and import it inside a CC3200 project in Code Composer Studio?

3. Can we connect a Speaker and stream audio from the Internet ? Is this DSP capable of doing this ?

4. Continuously keep listening on mic for a keyword like OK GOOGLE or HEY SIRI ?

5. I have this Booster pack http://www.ti.com/tool/CC3200AUDBOOST and I am yet to figure out how this Works ? 

I am sorry for this noob type questions because This is my first experience with Audio processing hence i beg your pardon ?

Regards

Shashank