This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RC4560: Supply of +30V / GND instead of +/-15V ok?

Part Number: RC4560

I am wanting to take a schematic that uses the RC4560 which is supplied by +/-15V and instead use +30V / GND as the +/- supplies since the guitar amplifier I am making the circuit for can generate the +30V but nothing negative.

Does anybody know if the OPAMP will work with this supply setup?    I am assuming it will since the overall differential voltage is the same.

I understand the surrounding circuitry will also have to change, but my main concern is blowing up the OPAMP with the +30V/GND supplies.

Thanks.

Tim