Hi team,
The customer needs to develop the IP voice telephone. He would like to select an audio EVM board and an audio IC.
1. For the EVM board, here are the specific requirements:
a). There are two products to develop for the customer. One is the audio signal is input through the mic and the audio signal is output through the speaker.
Another is the input audio signal and the output audio signal are connected to the analog audio data for four-wire telephone.
The board can handle the audio input and output, support for analog-to-digital audio conversion.
b). The board can run the Windows system or the Linux system.
c). The board should have the ethernet interface.
d). The board can be connected an external key to input.
e). The board should have this audio IC that the the signal input pins can be configured high and low voltage level.
f). Ambient temperature:-40C~85C.
For the audio IC, another product is the input audio signal and the output audio signal are connected to the analog audio data for four-wire telephone.
The customer would like to select an analog-to-digital audio conversion IC for the four-wire telephone.
Can you recommend a suitable EVM board and an suitable audio ADC IC?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments