This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM3070: adaptive mode

Part Number: PCM3070

Hello

 

My customer is designing  the software  for pilot-run of Audio-productt using PCM3070.

 

My customer is using 3 volumes.

Two volumes (L/R)  i2c register is in Page 44, and main volume is in Page 45.

It was located by GDE automatically.

Anyway

When customer want to change the main volume (Page 45 volume) , as adaptive mode, 

customer should use  Page 44 Register 1 in order to swap the coeff?

We know i2c logging and  we should switch ( swap ) the buffer for change the volume.

 

I did not find "DAC coeff buffer switch" in Page 45, so, even the components (main volume)  is

in Page 45, I recommend customer to use Page 44 Register 1 in order to swap.

Is it correct?

Best Regards