This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204: on the document SLAA557

Part Number: TLV320AIC3204

Hi all

Would you mind if we ask TLV3204AIC3204?


<Question1>
There is the description "5.2.1 Page 0 / Register 0: Page Select Register - 0x00 / 0x00 (P0_R0)" on the document SLAA557 P96.
What does it "Summary of Memory Map" mean?
It means "Summary of Register Map", doesn't it?
(It is the same as "Page 1 / Register 0: Page Select Register - 0x01 / 0x00 (P1_R0)" on the document SLAA557 P123.)

<Question2>
There is the description "5.2.16 Page 0 / Register 16: Reserved Register - 0x00 / 0x10 (P0_R16)" on the document SLAA557 P99.
We guess that usually Reserved Register allows to read only.
Why can this register write? And what purpose does it use for?


Kind regards,

Hirotaka Matsumoto

  • Hi, Matsumoto-san,

    1.- You are correct. There's a typo in "5.2.1 Page 0 / Register 0: Page Select Register - 0x00 / 0x00 (P0_R0)". It should be "Summary of Register Map".

    2.- Thank you for this observation. This is also a typo in the datasheet. It should be marked as read only (R).

    Thank you again for these observations. I will notify the team in order to modify this content.

    Best regards,
    Luis Fernando Rodríguez S.